logo

25 years of pressure transmitters
REFRIGERATION AND AIR-CONDITIONING
CONTROLS

By Arne H. Blom,
Product Manager
Danfoss developed the first pressure transmitters more 
than 25 years ago, but it was not until the 1990s that the
refrigeration industry began seriously considering the use 
of these electronic units. Customer demands for accurate
regulation, the need to reduce energy consumption and 
legislation requiring the registration of temperature 
throughout the entire refrigeration chain were the tasks 
that could not be performed without pressure transmitters.
Electronic pressure transmitters in a refrigeration plant 
are able to convert any pressure to an electrical signal. 
This signal – a voltage, a current, or in digital form – can 
then be sent to a control unit situated either in the 
immediate vicinity of the refrigeration plant or in a central
station at a service company perhaps many hundreds of 
kilometres away.

How to contact Danfoss

Danfoss button One level up